Part Number: SN74LVC1G240 Other Parts Discussed in Thread: SN74LVC1G04 , , SN74LVC1GX04 , SN74LVC1GU04 Hello,
I have a user seeking support for a recommendation for a 32kHz Pierce Oscillator:
I am seeking some technical help regarding the use of…
Other Parts Discussed in Thread: SN74LVC1G240 We are using the SN74LVC1G240 in the DSF package. Pin 5 is labeled as no connect. Does anyone know if this pin is connect to anything internally on the part? Can this pin be tied to VCC or ground?
Thanks…
Other Parts Discussed in Thread: SN74LVC1G240 Hello Everyone,
I want to know if this "little logic" gate, is an INVERTING or NON-INVERTING buffer, because in the product page
http://www.ti.com/product/SN74LVC1G240
it is referred as non-inverting…
Other Parts Discussed in Thread: SN74LVC1G126 , SN74LVC1G240 , SN74LV125A Hi all
Would you mind if we ask SN74LV14APWR, SN74LV125A, SN74LVC1G240 and SN74LVC1G126?
<Question1> These datasheets show min and max value of tPLHD and tPHLD(tPD). So, do…
Part Number: SN74AUP2G240 Other Parts Discussed in Thread: SN74LVC1G240 Hi team,
Is there any varient of the PN: SN74AUP2G240DQER, with temperature range of '-40 °C to 125 °C.
Please suggest an active alternate with the above part specs and with recommended…
Part Number: SN74AHCT1G04 Other Parts Discussed in Thread: SN74LVC1G240 Tool/software: To the person in charge
About 4 Pin Configuration and Functions of Data sheet,
In the pin layout diagram on P3, pin 1 is NC and pin 2 is A, but in the layout diagram…
Part Number: SN74LVC1G04 Other Parts Discussed in Thread: SN74AUP1G04 , SN74AUC1G04 , , SN74LVC1G240 The datasheet specifies "data retention only" down to 1.5V. Our understanding is that this means that the circuit will hold the output at the same level…
Part Number: MSP430FR2000 Other Parts Discussed in Thread: MSP430FR2111 , SN74LVC1G240 Dear,
as below code picture, the debug is normal, but after program, it may restart when character i =4,could you help me check what is wrong with it.
//**…