Hi Patrick,
This may also be a question more appropriate to the IBIS modeling team, but I'm fairly certain you can't simulate IBIS models using TINA. For that, you would need a spice model. Again, this is something we can probably provide if we know…
Part Number: PCA9555 Other Parts Discussed in Thread: SN74LVC1G57 , SN74LVC1G123 HI sir,
We now have a CPU connect the reset pin on PCA9555 P16, but when we enable the reset function (set the P16 to Low) the CPU cannot perform actions.
The reset…
Part Number: SN74HCS7266 Other Parts Discussed in Thread: SN74LVC1G57 , SN74AUP1G57 We're looking for the 1ch XNOR similar to SN74HCS7266 in one package device. is there good device you can recommend?
Regards
Brian W
Part Number: SN74LVC1G123 Other Parts Discussed in Thread: SN74LVC1G57 All 8-pin package monostables have only Q as output and Q is a positive pulse. I'm looking for a small package, such as the DSBGA (8) 1.91 mm × 0.91 mm, but with /Q output; IOW, a…
Part Number: SN74LVC1G07 Other Parts Discussed in Thread: SN74LVC1G32 , SN74LVC1G97 , SN74LVC1G57 Hi Sir,
May I know if we have buffer with enable pin control?
I need non-inverting, open drain output and one channel buffer.
Thank you.
Hi Tim,
Some background: Almost all of PSpice models available on the web currently were automatically generated. So any that weren't will have to be manually created by me.
If you'd like, I can get started on creating the models for the SN74LVC1G57…
Part Number: SN74LVC1G97 Other Parts Discussed in Thread: SN74LVC1G57 , TINA-TI Has anyone sucessfully used the SN74LVC1G97 (or 1G57) as a gated oscillator? Asking as I can't simulate it due to the lack of a Spice model for TINA.
Just 2 Hz is the goal…
Hi Kranthi,
I can submit a thermal modelling request to get these values for you, however the soonest I would expect results would be about 2 weeks (4/18).
If you need something sooner, you can use the thermals from the SN74LVC1G57 for an initial…
Hello Shu-Cheng,
" Schmitt trigger action " -- which is what the above datasheet says (not " Schmitt-trigger inputs ") is a marketing term to indicate a slightly improved tolerance to slow inputs. The Nexperia 74LVC1G08 does _not_ have Schmitt-trigger…
Hi Jim,
We have a few " configurable multi-function " logic gates. Such as the SN74LVC1G57 . However, they all have the same pin layout and will not be a P2P replacement as they need 3 inputs to have configurability (see below).
If you need to have…