Part Number: TAS2563 There are many registers that are mentioned in the datasheet description text but are not included in the register map.
For example the LIM_MAX_ATN, LIMB_TH_MAX, LIMB_TH_MIN, LIMB_INF_PT, DVC_RAMP, DVC_PCM registers.
Is there…
Part Number: TAS2563 Hi,
We are using two TAS2563 IC interface spakers in our product.
I have belwo questions to understand more:
When our device is shutdown only VBAT power is present and VDD & IOVDD is off. In this case, the register configurations…
Part Number: TAS2563 Hi Team, We are desiging audio section with TAS2563. In the layout for better power routing we going to connect at Pin1 (NC) with 3V3 supply and Pin 17 (NC) with VBST. Can you please confirm that if we can use the same or does this…
Part Number: TAS2563 we have a query now related to the sampling rates as below: 1. HFP is supporting 8KHz from the host but will the amplifier be able to support that sampling rate? 2. The A2DP of my host is giving 44.1Khz sample rate at mono 16bit so…
Part Number: TAS2563 Hello Team, In the TAS2563 datasheet introduction section, some voltage values are given for VBAT and PVDD as per the below image.
For PVDD supply, two provisions are there: 1) up to 13V and 2) up upto 15V. Both are QFN packages…
Part Number: TAS2563 Tool/software:
Hi TI Team,
We are currently working on integrating the TI ADC (TAS2563) with the XMOSf3800. At the initial stage, the device status appears to be in shutdown, and we are enabling it by writing register 0x02 to…
Part Number: TAS2563 I am using two TAS2563 amplifiers on the same I²C bus. ADDR_SPICLK is wired so that:
One device = 0x4C (pulled low)
The other = 0x4F (pulled high)
An I²C scan correctly shows both 0x4C and 0x4F, so addressing works…
Part Number: TAS2563 Tool/software: Hello-
I just want to confirm the voltage thresholds and voltage limits for the SDZ pin of the TAS2563. I am planning to use 3.3V logic and power for IOVDD, and 1.8V for VDD. Is SDZ considered a digital or analog…
Part Number: TAS2563 Tool/software: Using the PurePath Console 3 to get config register values based on my speaker and project. The output of that is below. The example C code for how to write those registers via I2C is very confusing IMO and I would…
Part Number: TAS2563 Other Parts Discussed in Thread: TAS2562 , TAS2781 We are working with a system using the QCS8550 chipset and TAS2563 amplifier, connected as shown in the attached schematic. I2S has been used for audio data transfer and I2C for the…