Part Number: TAS5760M-Q1 Other Parts Discussed in Thread: TAS6511-Q1 , TAS67524-Q1 Hi,
I would like to know whether the TAS5760M-Q1 provides any built-in mechanism to detect if one of the speakers is disconnected (open-load condition).
I need to implement…
Part Number: TAS5760M-Q1 Other Parts Discussed in Thread: TAS5760XXEVM Hi Team,
I am using the TAS5760M-Q1 amplifier in my design and have purchased the TAS5760xxEVM for development purposes.
We are planning to replace the existing TI amplifier (TAS5806MDCPR…
Part Number: TAS5760M-Q1 Hi All,
I'm currently working with a Linux-based device on an ARM architecture, specifically running kernel version 5.15.71 . I'm looking to interface an Audio amplifier with part number TAS5760M-Q1 to this device. Could someone…
Part Number: TAS5760M-Q1 Other Parts Discussed in Thread: TAS5720A-Q1 Tool/software: Hi team,
Would like to have a quick check with you. Previously, customer used both OUTA and OUTB channel. But there have some requirement change which only require…
Part Number: TAS5760M-Q1 Tool/software: I need to distinguish if the onboard amplifier is the TAS5720 or the TAS5760. Is it possible to distinguish the TAS5720 from the TAS5760 via I2C? The "Device Identification" register value is 0x00 for both devices…
Part Number: TAS5760M-Q1 Other Parts Discussed in Thread: TAS6422-Q1 Tool/software: Hi team,
Customer met some problems that there is a probabilistic communication failure on I2C configuration for bothTAS5760M-Q1 and TAS6422-Q1.
Below is the startup…
Part Number: TAS5760M-Q1 Tool/software: Hi, Team
I know when TAS5760 set to hardware mode, SPK_SLEEP/ADR is used for SLEEP function, and if the TAS5760 set to software mode, users can use SPK_SLEEP/ADR pin to set the i2c address.
But my customer prefer…
Part Number: TAS5760M-Q1 Tool/software: Hello,
I am working on TAS5760M-Q1.
At the power up, I set the following registers :
REG ADDRESS
DATA
0x02
0x04
0x01
0xFD
0x06
0x51
The others are kept as default…
Part Number: TAS5760M-Q1 Hi TI team,
We have requirement for class D audio amplifier for automotive application.
It should driver x2 5W, 8 ohm speakers.
Audio type Stereo.
Also, it should support load diagnostics
TAS5760MTDAPQ1 , meets above…