Part Number: THS4631 Other Parts Discussed in Thread: OPA810
Hi Team,
Good day.
Our customer is designing a protection circuit against short term overvoltages of a Howland current source realized around a THS4631 OpAmp. According to the datasheet…
Part Number: THS4631
Hello Support team,
I want to know more detail regarding below post.
THS4631 input bias current - Amplifiers forum - Amplifiers - TI E2E support forums
I've built a circuit similar to the one in the previous question.
…
Part Number: THS4631 Other Parts Discussed in Thread: THS4531 Hello Support team,
I want to know more detail regarding below post.
Could you let me know about more detail structure what ESD diodes used to protect the input from differential over…
Part Number: THS4631 Our design uses THS4631D Op-Amps.
In two of the instances of the unity gain configurations, the output is oscillating.
Output is connected to a trace of < 100pF (10”) which is not terminated at the far end. The far end is connected…
Part Number: THS4631 Other Parts Discussed in Thread: OPA810 , OPA857 , LMH32401 Hi sir,
I have a technical problem on ths4631.
when testing the output port, the difference between the test value of 1us and that of 51us is 14uv. How to modify the…
Hi Tatarao,
a DVM can show a huge input capacitance destabilizing the THS4631 by too high capacitive output loading. This is often overlooked when connecting a DVM directly to the output of OPAmp without introducing a suited isolation resistor. Usually…
Part Number: THS4631 Other Parts Discussed in Thread: TINA-TI Hello,
I am using the THS4631 configured as a differential amplifier with very low gain = 1/40 = 0.025 and high resistance values, which might be the cause of the oscillation I am seeing…
Part Number: THS4631 Other Parts Discussed in Thread: OPA810 , , OPA656 Hi Experts,
There are several explanation about recommended decoupling capacitor for Vs on the datasheet.
P14: Minimize the distance (< 0.25”) from the power matched impedance…
Part Number: THS4631 Dear TI expert,
I design a PCB in which a THS4631-based integrator is used. The circuit is as Fig1. The power supply for 4631 is +16V and -12V, feedback capacitor C2 is 20pF, R1 is 100 ohms, which leads to high output voltage slopes…
Part Number: THS4631
Dear Ti expert,
I consulted you a problem about the configuration of peak detector several months ago.
e2e.ti.com/.../940064
I followed the circuit shown by Kai in the thread above, and it worked perfectly.
When I remove…