Part Number: TLV2172-Q1 Other Parts Discussed in Thread: TLV172 Hello Mike Hartshome:
Indeed the model attached runs with .01uF.
There is no need for it to drive high cap..
thnx
robin2_tlv217_drven.TSC
close this post after you review.
Part Number: TLV2172 Tool/software: Can you please tell me how to calculate to total output error for this amplifier. If i gave 5v input to this amplifier, what will be the exact accurate output voltage after subtracting all the errors.so, provide detailed…
Part Number: TLV2172-Q1 Hello:
Pl see the schematic attached.
We are trying to get approx 4mA current thru rx.
Clearly, by setting vx, as an example, to 2.25v, rx=560 Ohm, we expect Vx to track vr. Thus bridge's total current will be 4mA.
But…
Part Number: TLV2172-Q1 Hello Team, my customer has following question:
In the datasheet (SBOS784C –NOVEMBER 2016–REVISED JANUARY 2019), short-circuit current is defined as shown below.
I want to make sure that my understanding is correct, and I was…
Part Number: TLV2172 Other Parts Discussed in Thread: TINA-TI Hi team,
1. Customer feedback is as follows:
The customer produced a batch of products (317pcs) and reported a total of 5 sets of equipment with performance failure. One of them reported…
Part Number: TLV2172 Hi Team, Our customer is using TLV2172 to drive a piezo sound element. It works during normal conditions but when the piezo element suffers mechanical shocks, it generates electrical surge to the amplifier. What would be the recommended…
Hi, Paul.
The heatsink is connected to the collector of TIP42, and I've found the root cause of the short path. It's the oscillation in the TLV2172 due to floating voltage at pin 5. after adding pull-down resistor on the pin, the issue is solved.
…
Hi,
Thought the output swing says it is 70mV less than VDD, actually in this case the scenario is limited by the input common mode range of this op-amp which is about 2Vs from VDD (as mentioned in datasheet)
Hence it is somewhere around 5.6V.…
Hi,
You don't need to download anything more.
You can directly copy and use the already placed macro from Ref-Design file in you design file .
Or you can Go to Insert --> Macro , to choose and insert the .TSM file downloaded(in the zip package…