Part Number: TLV6713
Hi
at the datasheet the pin SENS as input current of max 25nA ,
When i use the Pspice model TLV6713 the input current in pin SENS is about 400nA ,
What is the value that reflects the real situation? 25nA or 400nA
If…
Part Number: TLV6713 Other Parts Discussed in Thread: LMP7300 , TL7712A , TLV6710 Hi team,
My customer is looking for a comparator. Does TI have a comparator with the same function as TLV6713, but it is inverting?
He created a Sealed Lead Acid Battery…
Part Number: TLV6713TLV6713 has a built-in hysteresis. To increase the hysteresis, can I add a feedback resistor from output to the non-inverting input just like a standard comparator?
If the internal hysteresis is done by adding the similar feedback…
Part Number: TLV6713 Hi,
When I try to create a macro file using the TLV6713.lib in TI-TINA, I'm getting an error saying 'Missing Syntax Element - Line #43'.
Please could you verify the .lib file for any syntax errors?
Thanks for your help.
Part Number: TPS61094 Other Parts Discussed in Thread: TLV6713 Tool/software: There is a new generation of supercaps (Lithium Ion based) and I would like to know if we could use these instead of regular super capacitors with TPS61094? One example is this…
Sato-san,
You can use the TLV6713 comparator with 400mV reference (falling threshold) and use a level shifter (see Fig 10b in app note snva856) to interface to the EN/UVLO pin of the LM5145.
However, the hysteresis is only 5.5mV (1.35%) or 270mV…
Hello Dan,
The TLV6710 and TLV6713 outputs can be pulled-up to 25V (28V Abs Max) regardless of supply voltage.
The datasheets have been corrected and will be going through sign offs for release. Hopefully the corrected datasheets should be on the…
Yes, using a combination of high voltage micropower opamp, comparator, voltage reference would be solution design over-voltage protection ciruit.
For example, the TLV6713 Comparator is 36V and it has internal 400mV reference. TLV1701 is also 36V, micropower…
Abhishek
Unfortunately the circuit implementation you shared will not work. The LMP7300 input common-mode voltage range is from1 V above the negative rail to, and including,the positive rail. Generally the REF pin or a resistor divided down version…
Part Number: TLV6703 Other Parts Discussed in Thread: TLV6710 , Team,
-Is it possible to use the TLV6710 TINA model for simulating the TLV6703? -The overall electrical specs are very close so I guess that it could be realistic to do so. What do you…