Part Number: SN74CBT3125C Other Parts Discussed in Thread: TMUX1511 , TMUX1574 , Hi,
I am looking for a smaller SPI level shift solution. The application include a "motor driver” that communicates with “host controller”. SPI voltage for driver is 3…
Hey Jason, The highest bandwidth 8:1 we have is the TMUX1308 with a bandwidth of 500MHz. What's the application here? Are we looking for 1GHz per line speed or is this something where 1Mb of information is sent across all the signal paths collectively…
Hello Dakotah-san,
Yes, it is 3.3V for the MUX.
But the customer does NOT want 3.3V present when supply voltage is 0V.
I understand that the TMUX1511 the right choice here.
Appreciate your help!.
Regards,
Itoh
Hello,
Thanks for providing the expected output. What output are you currently experiencing, that you earlier mentioned was not expected?
Additionally, I would like to recommend replacing this part with TMUX1511, which has the same functionality and…
Hello Malsekar,
The TS3L4892RHR has a bandwidth of 1.1GHz which I am afraid won't be enough for your application. Can you please clarify what do you mean about " (I reckon it might be 4Gbps itself)"?
From my understanding your are inputting four signals…
Hi Sébastien,
Thanks for providing the diagram! Sorting through all of the devices in our portfolio by bandwidth, I came up with an idea for your solution.
TMUX1511 is a high bandwidth switch with four individually controlled signal paths (4 channel…
Part Number: TXB0104 Other Parts Discussed in Thread: TMUX1511 , SN74LV4066A , TXU0204 , SN74AHC125 , SN74LV125A , SN74LVC125A , TXU0304 , TXU0104 Hi
i want to use TXB0104 for VCCA and VCCB use the same voltage 3V3.
is there any concern , thank y…
Hi Carlo,
I would also like to mention that we have a new pin-to-pin replacement for SN74CBTLV3125, which is TMUX1511, if you are interested!
Best regards,
Kate
Hi Hao,
The recommended operating conditions of TS5A21366 is -40~85C ambient. We have other SPST switches that is rated up to 125C.
TMUX1511 also SPST but rated -40~125C ambient temperature. This part also features 1.8V logic compatibility, Low Ron…
Hi Simba,
You can refer to this FAQ to calculate the Junction temperature of the device.
I would also recommend looking at our new TMUX1511 which is p2p compatible with the SN74CBTLV3126 and has additional features like 1.8-V compatible control…