Other Parts Discussed in Thread: DS92LV18 , TUSB1210 , TUSB3410 Background: I am trying to extend USB 2.0 function over 1000ft using TI's TUSB1210 and DS92LV18.
Can the DS92LV18 accept USB 2.0, are there any potential problems with this configuration…
Hi,
We are interfacing an FPGA between Motherboard and Pen Drive. We want to process the USB SCSI payload being transferred between motherboard and a pendrive / mass storage device.
Now the problem statement is when we want to initialize the device…
Other Parts Discussed in Thread: TUSB1210 Hello,
I am using TUSB1210 for my FPGA test and using the "output clock mode".
My FPGA using the ULPI interface to connect to the TUSB1210, and TUSB1210 will be plug by an usb wire to PC.
I can see that…
Other Parts Discussed in Thread: TUSB1210 We should to use ULPi interface from 3730 to TUSB1210 ULPI transceiver and next USB output from TUSB1210 to one dual port HUB. I will use only HOST mode. My doubt is VBUS pin of USB1210. Really. my TUSB1210 "can…
Thank you Naoh and Diego.
Here are my comments regarding 3rd Question:
3. How does the TUSB1210 report and handle an over-current or short circuit event? According to me, TUSB1210 does not have logic to detect over-curent condition. And also as it…
Hello Trong Le,
I searched for TUSB1210 drivers for Linux or Android, but it seems this drivers are not available.Refer to Android or Linux release notes to see if TUSB121x is supported. In other case it is needed, the customer to implement the driver…
Other Parts Discussed in Thread: TUSB1210 Hello,
I have a few questions with using TUSB1210 in the device implementation. I plan on using the ULPI input clock mode configuration and the device will be self-powered.
1. In a self-powered device configuration…
Hello Aaron,
1.- Yes you are right, the figure 10-1 covers both functionalities.
2.- I don't have any good suggestion, since there is no EVM for the TUSB1210 and these switches are not in our group.
3.- The recommended operation is for VBAT (as…