Dear All
Could you advice about attached schematic? I am worried about two points of follows. ・ The B side is not SoC in conformity with Wi-Link-6. ・ Unused pin is Open. (If it need Pull Up/Down,please let me know)
Thanks
Best Regards
Tomohiro…
Other Parts Discussed in Thread: TWL1200 Hi All.
We're considering the usage of the TWL1200 level shifter to connect a WiLink6.0 based WIFI+BT combo solution (with 1.8V I/O) to a host SoC that operates @ 3.3V levels.
WiLink6.0 requires a reference…
Other Parts Discussed in Thread: TWL1200 Hi, I'm looking for dimensions for the YFF package of the TWL1200. Dimensions D and E are missing from the drawing on page 32 of the datasheet.
Other Parts Discussed in Thread: TWL1200 Hello,
We ave using the TWL1200 to interface 3.3V SDIO to 1.8V SDIO. We are not seeing the full voltage swing on the 3.3V SDIO interface. Any thoughts on why it's not driving to the 3.3V rail?
Thanks in advance…
Part Number: SN74AVCA406 Other Parts Discussed in Thread: TXS0206A , TWL1200-Q1 , TXS0206-29 , TWL1200 , TXS0206 , TXS02612 Hello support member
# SN74AVCA406 MAX Clock speed
Checking the data sheet of SN74AVCA406, the MIN of Clock seems to be 52MHz…
Part Number: TXS0206A Other Parts Discussed in Thread: TWL1200 , TXS0206 Hi team,
My customer want a 3.3V ,50MHz SDIO redriver,
I see many of you proposing voltage translator like TXS0206 or TWL1200,
But aren't those translator and buffer? can…
Part Number: TXB0104 Other Parts Discussed in Thread: TWL1200 , TXS0206 , TXU0304 Hi Team,
Good day!
I would like to know whether the TXB0104 is suitable for a communication from a microcontroller to a microSDHC card in "SPI mode". The microcontroller…
Hi Khemraj,
I am not sure what the specifications of each of those signals are. I would suggest starting with the Buffer/Driver/Transceiver family of parts and then using the parametric search to narrow down the options here: www.ti.com/.../products…
Hello Stokes,
Besides the difference in maximum capacity there are also different speed ratings defined in the SD specification. These ratings can be found at the following link: and in the table below.
We can see that SD 3.0 can support data rates…