Part Number: PROCESSOR-SDK-AM62A Hello Team,
I was exploring AM62AX-SKEVM.
Like to know is there any benchmark report for boot time, GPU etc.
I referred the attached report but looking for boot time with peripheral initialization/Power ON.
BenchmarkReport_sprad90…
I also apologise for not explaining clearly. I try to achieve writing and storing key in the secure area that is mentioned in TRM document 12.5.6. Key Area Registers. I just tried to read in the debug mode. It is not my main purpose. My main purpose is…
Hi,
Can the AES 128 encryption on the CC3000 be used to encrypt a packet payload, or is it exclusively for smartconfig?
Based on the new releases from 1.9:
SECURITY module: --- NEW --- Optional module under #ifndef CC3000_UNENCRYPTED_SMART_CONFIG…
Other Parts Discussed in Thread: AES-128 On the Bluetooth IC’s (CC256x,4x), is the application able to use the encryption functions and AES hardware to encrypt/decrypt an array?
If so, how long does it take?
The application needs encryption at the…
Hi Jun, I have a question about the AT command of cc3235MODSF.
WiFi Frequency: 5GHz
WiFi authentication method
- Authentication protocol: 802.1x authentication
- Linkage method: WPA2 Enterprise
- Authentication method: EAP-PEAP MSCHAPv2
- Encryption…
Hi
I am trying to use cryptodev engine using openssl in OMAP4460. When I run the application I get the following error :
/ # openssl speed -evp aes-128-cbc -engine cryptodev invalid engine "cryptodev"
3069236400:error:25066067:DSO support routines…