Thank you for your reply.
I still don't understand why the delay from duty cycle update to motor voltage acquisition can be equivalent to zero order delay.
I think there are two possibilities: 1. The comparison value needs to be kept as a continuous…
Tyson,
the F2806x is not supported for the InstaSPIN-BLDC projects. You can certainly port it in yourself, but we don't provide an example.
You will see in controlSUITE some of the other projects are dual-built for F2803x/6x, so you can follow what…
Other Parts Discussed in Post: TMS320F28388D , C2000WARE , DESIGNDRIVE
自動車メーカーは電気自動車(EV)に多額の投資を始めていますが、 最近発表されたレポートによると 、EV市場は2019年の300万台から2030年までに2,700万台へと拡大すると予想されています。これは、21.1%の年平均成長率に当たります。このようなEV市場の成長に伴い、EV用の公共充電オプションの需要も急激に増大するでしょう。
EV充電ステーションは…
Part Number: TMS320F28379D Other Parts Discussed in Thread: CODECOMPOSER Hi Team,
We received this inquiry from our customer.
We want to program a TI C2000 F28379D using the Plexim PLECS Code Generation toolbox from www.plexim.com. We'd like to use…
Hello Brett,
I have gone through the documentation in quite a bit of detail and have made some good progress in understanding how this works. However, have one major disconnect in understanding how the input to the compare module is set. I have been…
You may find the code in pid.h in motorWare for PID controller, is independent with PWM using different function modules. You might refer to "fast current loop" as the link below if you want to implement a higher control bandwidth of current loops.
…
Hi,
TIDM-SERVODRIVE is based on a high voltage board DesignDRIVE-IDDK, part number TMDXIDDK379D
To use launch pad, we have single core (377s) launch pad, servo drive example available at
C:\ti\controlSUITE\development_kits\TIDM-SERVO-LAUNCH…
Other Parts Discussed in Thread: LAUNCHXL-F28379D , TMS320F28379D , DESIGNDRIVE , CONTROLSUITE , TEST2 , TMDSDOCK28379D Hello Everyone ,
W ith Two TMS320C28x 32-Bit CPUs and having a processing power of 200MHz, TMS320F283779D can be compared nothing…
Part Number: TMDXIDDK379D Other Parts Discussed in Thread: CONTROLSUITE Hello,
the above mentioned development kit offers the connection of an incremental coder via QEP. The circuit can be found in IndustrialDrivesRev[2.2].pdf on page 11. The document…