Have you provided any of the removed parts to TI for failure analysis. I've attached the form to fill out. It might also be good to furnish one or two IC's from the same reel which have not been put on your boards yet.
Other Parts Discussed in Thread: MSP430FG4618 Hello all. I was just wondering if someone can help post some tips for
my project. My project involves a flex sensor (potentiometer that
ranges from 60k to 100k ohms). Using external circuitry to send…
Part Number: MSP430G2533 Hello, can someone tell me where I can download the GUI software to let me view the data on the uart Interface?
I mean the green window in which the data is displayed (see attachment).
Best Retards
Janusz
7077.tidu546a…
It fails because the stdout is not displayed in the console or in the redirected output (also tried using the options -x log.xml --stdout-file=c:\stdout.txt). It is also not outputted to the textfile used by the fopen/fprint functions.
Here is the new…
Hi, I need to generate a very fast signal (40 KHZ) (which consists of an array of 0s and 1s) and this signal is sent to one of the GPIO pins on ez430-rf2500 board. This array is generated based on the values of the other array that is read from the memory…
Hi Norman,
Thanks, that was a good idea, but unfortunately does not change the issue. I will point out that the same boot-args work with the 2.6.34 kernel from the ezsdk.
Any other ideas?
The functional boot via 2.6.34 looks like this:
…
Revisited this and found ramdisk-base.gz from OMAP-L138_PSP_1_00_00_04\LSP\OMAP_L138_arm_1_00_00_04\DaVinci-PSP-SDK-03.20.00.05\images\fs.
Not sure why ramdisk-base.gz is not included in later PSP's.
>>Is there some kind of SPI Flash map conflict…
Hi all,
There was a fair bit of traffic overnight. Thank you for your thoughts! I'll repsond to each here:
But first I just wanted to restate my original question (which was not clearly stated in the first place) :
In implementing an interrupt…
Other Parts Discussed in Thread: CC2540 Hi - Please forgive the length below, but best to be explicit.
My goal: I'm trying to establish a siple BLE path from smartphone to a particular appliance we make many of each year. For various reasons, the appliance…
radioselect_usecasefiles.xlsx Hello Kenneth,
The .tgtcfg files, have a specific DFE configuration, the DFE configuration selects the:
IQN baseband configuration,
DFE Tx, Rx, Fdbk stream setup,
JESD and Serdes bit rate.
Within the RFSDK constraints…