Other Parts Discussed in Thread: TMP102 Hello,
I've got TMP102 breakout PCB where ALARM pin is left unconnected (no pullup). I'm not going to use ALERT pin anyway, but does it any impact on communication via TWI bus? I've tried to communicate with…
Part Number: BQ40Z50-R1 Hi
We have designed a BQ40Z50-r1 4S1P Battery Pack.
In this during Charging When the battery reaches CV mode ,the current starts to decrease but there is glitch in the Current. The Current is oscillating
Expecting the reply…
Other Parts Discussed in Thread: LM4040 I have a mature application using the National Semiconductor LM4040CEM3-5.0/NOPB. Recently within the last year my yield has decreased. The datasheet CTE is +/-20 ppm/C typical and +/-100ppm/C maximum. Part to part…
Part Number: CC1312R Tool/software: TI-RTOS Hello Gurus I'm using Ti 15.4 stack with with Linux based collator application, my default code is working and I'm getting sensor data at collector. In my application i need the data at interrupt and specific…
Derek,
The drop in voltage will never happen with the TPS25740 as it is a Type-C PD compliant device. But if a compliant device is connected to a non-compliant power source, then there can be potential failure as the sink device believes it is sinking…
Hello,
1V to 500V 100uA Boost Power Supply with TTL 32-bit Pulse Counter required for GM Counter. This being a standard application, it must be possible to manufacture a standard LOGIC level circuit with integrated analog part for voltage booster operating…
Thanks Wyatt for the explanation.
Attached you can find the .xlsx file where you can see how these parameters (DOD Passed Q, DOD Time, DOD0,QmaxDOD0, QmaxPassedQ and Qmax Time) become 0 when full charge is met. (row 1136 in file) bq34z100_SoH_calc.xlsx…