PS: E3 Schematic attached. PROC100E3_SCH.pdf
I recommend you probe VUSB_MAIN on TP28 and GND for starters to verify you're getting power from your power adapter.
Best,
Andrei
Part Number: BQ28Z610-R1 Other Parts Discussed in Thread: BQSTUDIO Dear Sir,
when charge complete BATTERY VOLTAGE is swapping repeatedly between from 4.16V to 3.9V.
please check GG file and Log file and let me advise me why it happened.
BQ28Z610…
FYI, I downloaded the ISSI data sheet and reviewed your spreadsheet. I saw some issues in your earlier spreadsheets but it looks like you've corrected them now. Once I get the full csv file I'd like to compare that against the spreadsheet to make sure…
Hi Jerome,
I'll have to check on the first two questions for you.
BRUNEAUX Jerome said: Is there any way by HCI events which can help to link the SCO used PCM audio channel to the BT connection ?
Have you seen the HCI_VS_Write_CODEC_Config (0xFD06…
Part Number: LDC1612 Hello
Why is the calculated frequency in the LDC161x-LDC131x_Config tab so different from the calculated frequency in the Spiral Inductor Designer tab?
As an example, the frequency(Inductance) result at d=1.5 mm is as follows…
Hi Guanming,
I apologies for missing your previous reply. Let's continue our discussion here.
I am first replying to old questions and then new ones. If the old queries are resolved, please ignore them.
1. After adjusting the output resistance,…
HI Adalbert,
The "assisted mode" just means that the CC2564MODA is interfacing with the audio codec instead of the host interfacing with the codec:
We have some information in the HCI_VS Guide for the CC2564x platform: 4370.CC256x VS HCI Commands…
Howdy Makoto,
snlu131_DS90UB928_EVM.pdf
This is the latest User Manual for that EVM. Can you please confirm this is the one you are using?
Thanks,
Holly Roper