Part Number: THS4303EVM Other Parts Discussed in Thread: THS4303 I am wondering if my THS4303 EVM is potentially defective. My set up is described below:
- I have a simple power supply circuit giving (according to a voltmeter) +1.8 V and -1.8 V relative…
Other Parts Discussed in Thread: THS4303EVM hello:
i want to amplifi a small negetive signal with amplitude=-10mv, rise_time=8ns, fall_time=30ns and width=40ns. my supply voltage is vs+=2.5v, vs-= -2.5v .
according to the datasheet of ths4303evm i…
Thanks Alec. One more request. It is also said that S-parameters are "(Measured using standard THS4303EVM, edge number 6454762, with VS = 5 V in a 50 Ω test system)". But I guess only the opamp is measured, so there has to be some kind of correction,…
Part Number: THS4303 My setup:
Using THS4303EVM with a Rigol DSA-815 Spectrum analyzer and Tracking generator (TG) sweeping from 1Mhz to 1.5 Ghz. The THS4303EVM input is connected to the TG and the output is connected to the spectrum analyzer input…
Part Number: THS4303 Other Parts Discussed in Thread: THS3491RGTEVM , THS3491 Hi Team,
I would like to request please, if possible, to receive the gerber files for the following evaluation boards:
THS4303EVM
THS3491RGTEVM
Also, if you know of…
Part Number: THS4303 I am interested in use this op-amp for a Negitive Impedance Converter (NIC). I have removed the terminating R to gnd . Does the non-invert need a R to GND to operate. I do not get the expected results from the THS4303EVM, compared…