Part Number: AM4372 Hi E2E
I would like to continue these topics because it should be one topic
https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1009372/am4372-xds200-tune-ddr-what-type-of-jtag-pins-to-use-for-it?tisearch…
Part Number: TMS320F280049C Hi Champ,
I am asking for my customer.
The customer is trying to connect the control card with XDS100v2 USB Debug Probe.
That, it is always showing : Error connecting to the target: (Error -151 @ 0x0). The message is…
Part Number: RM57L843 Hi!
I have been using the XDS100v2 debugger to connect to RM57 for flashing and debugging purposes. Unfortunately, the "Test Connection" fails every time I do the Integrity test. I have verified the hardware connections as per…
Part Number: CC2650MODA Other Parts Discussed in Thread: MSP432E401Y , MSP-EXP432E401Y Hi there,
We have a custom made board that includes an MSP432E401Y as main core and a CC2650MODA module to provide bluetooth connectivity. On this card, there is…
Part Number: TMS320F28069 There is an issue with my firmware I need to resolve. When I encounter that bug I bring the board back to my development system and connect the XDS100v2 Jtag module to my board and Click "Run" -> "Connect target"
This action…
Part Number: TMS320F28069M Other Parts Discussed in Thread: MOTORWARE , Hi team,
after debugging and running the modified motorware lab12b code on the F28069M I needed it to work without connecting it to the XDS100 stick. But it seems that after disconnecting…
Part Number: TMS320F28388D Other Parts Discussed in Thread: UNIFLASH Good afternoon,
We are using the F28379D control CARD for developing our own SiC motor drive. We are ready to lay out our own controller board using some circuits from the above…
Tool/software: Code Composer Studio Hi,
I want to program and debug the F28335 dsp by XDS100v2 jtag.
Does XDS100v2 work with CCS v9.1 and Windows 10 64 bit?
Regards,
Pouriya
Anil Garg said: After lowering the TCLK at 100kHz , Now its programming..
Good to hear. I assume you are plugging a USB cable between the PC and IDK to use the on-board XDS100v2. There is some stability issue with the connection that lowering TCLK helped…
Part Number: TMS320F28379D
Hi Team,
My customer is trying to get the data in the TMS320F2837xD i n real time to use debug probes.
They have the XDS100v2 that is no longer available.
Is the performance of the sample rate by…