Other Parts Discussed in Thread: TLV3604
Hi,
I want to connect an APD module to in+ on TLV3604EVM and lowpass filter the APD module and supply that to in- as a threshold which will vary with the DC output of the APD module. I then want the EVM to act as a comparator and output LVDS determined by whether or not the input to in+ is above the threshold in-. I know that to look at the LVDS signal on out+ on an oscilloscope I need to connect a 100 ohm resistor to R4 but I'm not sure what to do with the other resistors, does the board come with 0 ohm resistors as standard and should I just leave these as is?
Cheers,
Shaun