Other Parts Discussed in Thread: ADS5296A,
Hi all,
I need to drive the ADS5296A (10b/12b) with signals from around 200kHz up to 80 MHz through a VGA which is driven from single-ended source.
I will be using the ADC mainly in non-interleaved mode but maybe in the future go to interleaved.
Thought of the THS7530 with almost-DC coupled SE input and differential output.
The gain adjust of THS7530 is sufficient for me.
Is this is reasonable choice or is there a better alternative?
Thanks
David