Part Number: INA240
Other Parts Discussed in Thread: DRV8312
Hi
I have a question about INA240A1.
I am using INA240A1 in DC brushless motor circuit to measure motor current value.
When measuring the current on the high side of the motor, the output of the INA240A1 is not stable and I am in trouble.
This phenomenon can be observed both by simulation with PSpice for TI and by measurement with an actual oscilloscope.
This phenomenon occurs when the PWM frequency is set to 100kHz or higher, and when the PWM frequency is set to 10kHz, the Hi-side side can also be measured correctly.
Please check the attached document for details.
Question
- Do you understand why the low side current can be measured stably and the high side current fluctuates?
- Are there are any limitation of PWM frequency value when using INA240 ?
-Are there any alternative ICs for measuring high-side current values in the attached file's condition?
Best regards
Naoki