Other Parts Discussed in Thread: OPA692, OPA3692, , OPA3693
I'd like to make a circuit with fanout analog signal 1:8.
First page of OPA692 shows circuit correspond our requirement, just adopt 2*OPA692
Lately, I found OPA3692 has 3 channel, maybe I could implement like:
But I have a 2 problems:
(1)
The output current for both the OPA3692 (3ch) and OPA692 (1ch) in the datasheet is 190mA.
OPA692 use 190mA, no problem.
Is OPA3692 190mA per channel or 190mA/4 per channel?
(2)
I also discover OPA693 which has similar configuration, but it only drive 2 channel(datasheet)
and max output of OPA693 is 120mA, which is about half of OPA692.
So I guess to drive "sufficient" current, it should be 50mA per output channel.
(50 ohm terminated and RG316 cable)
Right?