Other Parts Discussed in Thread: TLV4051, TLV4041, TL331, TLV7011
Hi Team,
The main power input in my design is 12V. I need to monitor this 12V power and generate the PGOOD signal using a comparator with hysteresis.
The comparator should generator power good when supply voltage is more than 10.5V. The comparator output is connected to a FPGA which can accept voltage level of 3.3V.
Can you please suggest me a comparator (with hysteresis) part number which can be used to monitor input voltage of 12V and generates output voltage that can be connected to a 3.3V IO signal.