Part Number: TLV7032
hi team,
Once of our customer is currently evaluation TLV7032DSGR.
Could you kindly have a quick look into below customer question(s) and help providing feedback?
I have some questions regarding the TLV7032DSGR, which could be a good option for one of our products:
- For simplicity we want to use this comparator with a reference voltage of Vcc and a signal which moves around Vcc and therefore, can also be higher than Vcc.
- According to the datasheet the recommended input voltage range goes up to Vcc+0.1V, but the absolute maximum rating goes up to 7V. Therefore, I assume the inputs are not diode-clamped to Vcc. Can you confirm that?
- Anyway, the current through the inputs is also limited by external resistors to a maximum of a few µA.
- I tested the circuit also with input voltages of up to Vcc+2V (before the current limiting resistor) and a reference of Vcc. The circuit worked without problems. Do you see any potential risk if we use the comparator this way?
Thanks!
Regards,
Brian