Part Number: LM393LV
Hi,
May I ask if VIN+ VIN- and Vout can withstand 0-6V voltage when VCC is not powered?
Many thanks!

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Rhea,
Yes! The LM393LV has "Fault Tolerant" inputs, that can go up to 6V without damage, even with the power off.
See section 7.4.3.2 in the datasheet apps section for more details.
As always, we recommend that input voltages be kept within the specifications during normal operation.
And, yes, output, too!
Hi Rhea,
I'm glad that you were able to find the answer you were looking for! Please click "This is resolved" on Paul's response.
-Chi