Other Parts Discussed in Thread: LM741, TL071H, OPA990
Hi, I need to know the replacement for LM107
is LM741 ??
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The LM107 is a 40 V opamp which allows input voltages up to the positive supply.
In general, possible replacements might be the TL071H or OPA990. If we knew the application and its requirements, it would be possible to give better recommendations.
Hi Carlos,
not to forget, the operating temperature range of LM107 is from -55°C to +125°C. Must the replacement also meet this specification?
Kai