Hi.
I've done a charge amplifier with the JFE150 and I've noted as the noise increases
as the input protection diodes are connected to + and - 6V used as power supplies.
Such a power supply voltages are on board and comes from a LT3042EMSE and a LT3093IMSE.
The JFE150 is powered between +6V and GND.
In the datasheet is not specified the capacitance of connected input diodes, where can I find it?
Thanks.