Hello TI community,
I've been using AFC2101 for a project, with great success but now I'm trying to improve my design. I use AFC2101 in switched mode and have a polypropylene (WIMA) S/H capacitor which is what my ADC samples on (also my test point for this post). I'm working to create a better absorbance detection unit -- I know a blank reading registers about 100 uA of photocurrent on a photodiode (I verified this with a Newport power meter), but this means (5 A.U. = 1 nA photocurrent, 6 A.U. = 100 pA).
I was interested in what leakage current works its way to input of AFC2101 amplifier so I disconnected the Switched Input A (SW_IN_A) and let the pin float. I set a very high integration time (100 millisecond) and then look at output voltage. From Page 9 of AFC2101 datasheet from TI.com I find nice equation to find output voltage with integration time.
These output voltages are taken from sampled output capacitor on a Fluke DMM:
If I integrate for 2000 microsecond I get output voltage +8.17 mV
If I integrate for 100 millisecond I get output voltage -10 mV
So for a delta time of roughly 98 millisecond I get a delta voltage of roughly 18.17 mV. Running from Page 9 I figure that this gives me approx a leakge current of 18.5 pA (18.5 PICOAMPS, very good).
So I have several questions:
1.) For low integration period (2000 microsecond) is this +8.17 mV "offset" from charge transfer and general mismatch in the 2101? How can I determine where the 2101 begins integration.. Datasheet says "The integrator output voltage range is from +0.5V to –10V." Does this mean I'm observing 491.3 mV of offset from my first integration.
2.) Is my method sane for determining bias current? I let the SW_IN_A pin float and then analyze two different integration periods. Another experiment I can do is when I get my PCB back from AC I'll put it in my dark Box with the photodiode. Currently, I can't seem to shield the photodiode well enough (even in dark enivorment there is always a 100 nA current, I did not reverse bias the diode).
3.) The datasheet says the AFC2101 has Bias current of typical 0.1 pA and maximum of 1 pA. In circuit designs like this how feasible is it to approach this limit? I'm very new to low noise circuit design but I've followed up with guarding ringing my high impedance nodes. Any other tricks? How can I quantify these measurements?
Sorry for huge post but TI staff and community is very helpful so please any help or discussion would be great.