I am now working with the same configuration, however, I am having difficulty getting the THS4509 to work with the ADC board. I have basically taken everything off of the ADC side path and jumpered with 0ohm resistors. I am using the differential outputs of the 4509 into the ADC. I have thought that I would need to connect the CM pin from the ADC to the 4509 CM control input, but when I do, the output of the 4509 goes to a solid 1.5vdc. Without it, I do get an output. With DC coupling, do I need to connect the CM pin? Do I need any special termination on that pin?
I have it connected in TINA and it seems to work. I did not change any of the values on the 4509 EVM. I am using a 50 ohm AWG at 50mVpp and 5kHz.
Anthony