Other Parts Discussed in Thread: LM224-N, LM224
What are my concerns if the LM324-N Tj operating temperature specification is reduced to -25°C?
(Is it possible to guarantee the temperature at -25°C to 70°C?)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Koichiro-san,
The requested temperature is outside of the recommend operating conditions, as Kai has stated.
Unless you are the sure the application will not exceed -25C, I would not use LM224 either, the margin is too low.
I instead would use either of the devices highlighted above.
Could you please share application requirements?
Most modern op amps have temperature range -40C to 125C, I recommend an op amp for the application.
All the best,
Carolina