Part Number: INA310A
Other Parts Discussed in Thread: INA190, INA293, INA301
Hello,
I want to drive 3 resistive loads with controllable current source:
- R1 = 6.5R; V1_max = 13V; I1_max = 2A
- R2 = 11R; V2_max = 14.3V; I2_max = 1.3A
- R3 = 400R; V3_max = 96V; I3_max = 0.25A
These are my inputs:
- V_in = +12V
- V_control = 0..2,5V (from DAC)
I can boost the +12V to +15V@4A (for R1 and R2) and +100V@0.3A (for R3).
Can you suggest the adjustable current source that can drive these 3 resistive loads?
I can build 3 separate current sources for these, that's no problem. It will be best if they use the same IC.
Ideally, they should be driven using high-side sensing, i.e with this INA310 (so that 1 pin of the load goes to ground).
Thank you very much in advance.
Best Regards,