Other Parts Discussed in Thread: INA237, INA240
Hi,
We are using the mentioned P/N for current measurement with the following scheme:

The sequence we are using is pretty straight forward:
- Setting Vout2_R to 9V -> Expected result are measured by the INA220
- Setting Vout2_R to 16V -> INA220 is stop working and can be recovered only upon a power down-up sequence of the platform.
Additional observations:
- Once we are in the transient from 9V to 16V we are experiencing the following wave form on the Vout_2:

It looks to us that the INA220 is failing to serve such voltage transient.
Are we correct?
Please let us know what we can do in order to improve the design.
Thanks,
Neta