Part Number: INA237
Hi,
My customer faced this question, which is given following:
INA237 owns the VIL which is 0.4V, and the low-level threshold of the front-end chip output voltage is also about 0.4V. So that they are worried about the threshold and margin.
And in the given e2e, which shows that INA237 is designed for the 1.8V I2C system: (+) INA237: VIL threshold confirmation - Amplifiers forum - Amplifiers - TI E2E support forums

Thus, my customer wants to know:
1. Whether they can make a power supply of INA237 as 3.3V, and the pull-up voltage source is 1.8V?
2. How can the power supply voltage domain and pull-up voltage source domain can influence the INA237?
For example, the power supply is 3.3V (main power), and the pull-up voltage source is 1.8V(standby power), the main power and standby power are different voltage source. Is there any influence? For example, the risk of the leakage.
Thanks and look forward to your reply.