The voltage and current sense gain errors are quite low (±0.01% typical, ±0.05% max), but the power total measurement error is quite high (±0.5% max).
Where is all this error coming from?
For my application, I'll be sensing (high-side) a 1A current through a precision 0.1Ω resistor (so 0–100mV shunt voltage) with 1–10V bus voltage. What kind of power measurement accuracy and precision can I expect (in mW)?
Also, it's a bit of a shame that there's no internal gain setting for the bus voltage; seems like we lose an awful lot of our precision by working at an eighth of the max.