This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA2376: Need a Dual source Amp

Part Number: OPA2376
Other Parts Discussed in Thread: OPA2392, OPA2325, OPA2397

I need to replace the OPA2376AIYZDR for a dual source amplifier with similar parameters (Noise, offset, rail to rail, drift, etc). My main request is the size. Would you have any Amp with similar size to this one?

Thank you. 

  • Lucas,

    Almost all op amps including OPA2376 do NOT have internal ground and thus may be used in a single, dual or asymmetric supplies for as long as the input and output signal voltage are within the linear ranges specified in CMRR and AOL datasheet conditions table.  Additionally, you may consider similar parts like OPA2392, OPA2397 and OPA2325.