Other Parts Discussed in Thread: RCV420, MAX232
Hello, I'm thinking to use the RCV420 to acquire a 4-20mA signal. Firts, this is my transmitter: http://www.prelectronics.com/idd956.asp?pcol=5333A, this transmitter has only 2 wire for the loop and the power supply and its supply voltage is 8-35Vdc, What is the correct connection between the transmitter and the RCV420? Second, Can I use the max232 to give negative supply to the RCV420? Finally, Is necessary that I give +10V to the 16 pin and -10V to the 4 pin?, Do these values affect in the output voltage? Thanks.