This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM7171: Input offset voltage drift

Part Number: LM7171

Hi all,

I'm looking at the LM7171A and need some clarification from the datasheet.

I suspect that there is a difference between the A and B version of the LM7171 (regarding the input offset voltage drift). 
If you take the specification from the datasheet: TCVOS: 35uV/C and compare this to the 2 figures in the datasheet:
Figure 5-3 (LM7171A) Input Offset Voltage vs Temperature, calculating the drift from this (+-15V): -40C=-1mV and 100C=0.2mV. This gives 1.2mV / 140C = 8.5uV/C
And figure 5-42 (LM7171B) Input Offset Voltage vs Temperature, calculating the drift from this (+-15V): -35C=2mV and 125C=-4mV. This gives 6mV/160C = 37.5uV/C
Given the large difference between the calculated value and the spec given on page 4 (TCVOS): Is this spec only applicable for device B or both A and B? 
What is the correct drift specification for device A? The graph or the number given in the datasheet?
Thanks in advance!