This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV9004: Output ESD protection

Part Number: TLV9004


Hi team,

We can find the ESD diode on the input pins has a torelance from the datasheet below.

 

Also we can estimate the ESD diode on the output pins also have a same torelance from the description below.

I'd like to make clear if we can take the both input and output of ESD diode specifications same?

Thanks.

  • Hello Sawamoto-san,

    You are correct, the input and output ESD diodes will possess the same limitations as mentioned in table 7.1 of the TLV900x datasheet. 

    Subnote 2 mentions that these didoes can tolerate voltages higher than that of the abs max table, so long as the current is limited to 10mA or less. 

    Please let me know if you have any questions,

    Best,

    Jacob