Other Parts Discussed in Thread: TLV9061-Q1, TLV9062-Q1
Hi
Can you suggest Q-grade and dual channel version of LMV796-Q1?
thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Can you suggest Q-grade and dual channel version of LMV796-Q1?
thanks!
Hello PYTSai,
I agree with Clemens, TLV9062-Q1 is close but has some key spec differences. Slightly higher max offset voltage, less GBW and slew rate, and higher voltage noise. I have provided a comparison table between the two devices below.

Do you have the application that this device is being used in so we may evaluate the best fit device?
Best,
Jerry
Hi Jerry,
If spec need to be equal or higher than LMV796-Q1, can you also recommend ? thanks !
Hello PYTsai,
We do not have a device that is better than LMV796-Q1 across every specification. This is why we ask for what the application is doing with the device, as not every performance specification may be needed.
Best,
Jerry
PYTsai,
Do you have a schematic or an input/output of the device? Typically liquid sensing is not a high-speed application. Are they applying a significant amount of gain?
If you would not like to share the schematic on the public forum, please send over email.
Best,
Jerry