Part Number: TL064
Hi support team.
If the supply voltage is Vcc+=+5.25V,Vcc-=-5V, will the value of KSVR get worse?
If yes,If yes, what should the value be?
Best regards,
Higa
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TL064
Hi support team.
If the supply voltage is Vcc+=+5.25V,Vcc-=-5V, will the value of KSVR get worse?
If yes,If yes, what should the value be?
Best regards,
Higa
Hi Higa,
The DC PSRR is not expected to be significantly different from the datasheet specification at the lower supply voltage if you are using at lower frequencies.

How much variation on the power supply are you expecting?
Regards,
Ashley
HI Ashley-san
You said : How much variation on the power supply are you expecting?
-> 10mVp-p/10kHz
Best regards,
Higa
Hi Higa-san,
I can verify what the PSRR difference will be in the lab for a small sample set but this be for information only and not guaranteed performance. I should be able to get some data by mid-next week and will update this thread.
Regards,
Ashley
Hello Higa,
In the data sheet, minimum CMRR and KSVR are the same and a DC spec. Therefore I would expect that a IQ vs supply voltage chart could be used to estimate the difference in CMRR and KSVR
Between +/-9V and +/-15V there is a 28 pixel difference. Between +/-9V and +/-5.125V there is a 29 pixel difference. Therefore it is reasonable to assume that offset change +/-5.125V to +/-15V is about twice the offset change +/-9V to +/-15V
The min spec is 80dB that represents a 1.2mV maximum change. Twice would be 2.4mV

For AC, compare the slope at 5.125V and the slope of 9:15
Pixel slope near 5.125V is 0.247 ; Pixel slope 9:15 is 0.247 = 0.124
Is not a surprise that AC PSRR should be half as good as 9 to 15V AC PSRR