Tool/software:
Hi,
I would like to use the INA233 to monitor Vcc and Icc. The connection is like this.
DC power supply -> Current sense resistor -> LPF -> DUT
The IN+ and IN- pins are tied to the both side of the current sense resistor. The VBUS pin is connected to just beside the Vcc input to the DUT.
Due to the small resistance of LPF, the max IR drop through the LPF is about 100mV.
Therefore, the voltage is VBUS < IN- < IN+.
Can I use in this way?
Thanks,