Other Parts Discussed in Thread: ADS8900B,
Tool/software:
Dear TI support,
In our custom data acquisition evaluation board we observed some unwanted behavior for signals with a few MHz. We tracked it down to the used PGA855 amplifier. For certain frequencies and signal strengths the amplifier becomes instable and produces ringing effects on the output signal. To ensure this is not caused by our design, we also bought the evaluation board of the PGA855 and are able to reproduce the same faulty behavior.
Here are 2 results of the PGA855 evaluation board supplied with +/-5V dual supply, 1Vpp input signal and Gain 1:
With 3.5 MHz we see a little ringing on the output signals (red, blue)

With 3 MHz we see a massive ringing on the output signals (red, blue)

Is this a (known) problem of the amplifier? Is this in any way related to the revision history of the datasheet where the maximum sampling rate was reduced from 4 MSPS to 1 MSPS?

But that doesn't actually makes sense because there was no change in the allowed input bandwidth (which should be 10MHz) but only in the sampling speed of an external ADC. What is meant by this reduction anyway - why shouldn't I be able to digitize the amplifier output signal with any speed I want to?
If you can confirm this behavior are there any plans for an errata of the datasheet or a new silicon revision of the PGA where this behavior is fixed?