Other Parts Discussed in Thread: LMV324,
Tool/software:
I am using a bandpass filter and a lowpass filter using an op-amp.
Until now I have used the LMV324, but this time I used the LMV324A.
There was a difference in the amplitude (peak to peak) of the waveform after passing through the bandpass filter and the lowpass filter.
Which characteristic of the op-amp causes this difference?
When I looked at the datasheet, there was a difference in the slew rate, but is this characteristic the cause?
(Reference) Measurement results
LMV324: 2.4V
LMV324A: 2.7V
(Reference) Slew rate
LMV324: 1.0V/us
LMV324A: 1.7V/us