Tool/software:
AMC3301 is used for AC-current sensing of a EV fast-charging station. I am looking for TI solution with similar spec. as AMC3301 but also with over current protection. Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
AMC3301 is used for AC-current sensing of a EV fast-charging station. I am looking for TI solution with similar spec. as AMC3301 but also with over current protection. Thank you.
Hi Freddy,
The output of the AMC3301 can be used to detect over-current if the input is sized to detect different thresholds. However, this is subject to the 3uS latency of the main signal path.
If a faster over-current detection is necessary they could consider using an isolated comparator in parallel, sensing across the same resistor.
Please see this application note for additional details: https://www.ti.com/lit/ab/sbaa605/sbaa605.pdf
It is best to run the AMC33xx device from a 5V supply on the low side in this configuration.