Tool/software:
I am using the following design to measure AC current:
The resistive values in the differential amplifier circuit are 15k, hence the gain is G = 1. This circuit should work according to the application notes, but the response I'm getting at the output of the filter, in the 'IOUT_MICRO' signal, is the following (This signal I should be obtaining should be a pure sine wave, since the load I've connected is a resistive load of 6A.) :
Replace R75 and R76 with a value of 0 Ohms and remove C55, but I'm still encountering the same issue. What could be happening?