Other Parts Discussed in Thread: LM339
Tool/software:
Hello,
As per LM2903AV datasheet: Sink current shows 6mA.
Please provide the Max sink current of this IC.
Regards,
Sudharshana
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Sudharshana,
There is really not a "Max" sink current, until you get to the current limit region.
The "Max" would be looking at the graph that Clemens displayed and finding the maximum VOL voltage that can be tolerated.
We recommend staying be;low 10mA.
See section 6 of the LM339 family appnote:
Application Design Guidelines for LM339, LM393, TL331 Family Comparators