Tool/software:
We have been using INA128s in one of our low volume products for more than ten years without any problems.
However, in our latest batch of boards we are having issues which are pointing at the INA128.
Our application is a test system and we use the INA 128 (G=50) to look for a small signal on one of the UUT outputs at times when the output is off. We also apply various switched loads to this output and use another INA to measure the UUT output when on and loaded.
As part of our system's selftest regime, a 100mA constant current continuity test (supplied at 28V) is used to test the values of the load resistors. On our latest batches of systems, these tests are failing with low resistance results, suggesting a parallel path through the INA128.
Looking back at the datasheet I used when I originally designed our circuit reveals the following Input Protection characteristics:
In the latest version of the INA128 datasheet is the following which suggests that the input protection has changed significantly.
Can you please confirm that I am correct, advise on when this change occurred and also advise on an alternative to the INA128 that has the old input protection characteristics?
Many thanks
Daren