This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDM-02014: OPA320AQDBVRQ1

Part Number: TIDM-02014
Other Parts Discussed in Thread: OPA320

Tool/software:

Hi TI expert,

In TIDM-2014, Could you please explain the circuit below:

Why Voutput is in range 0.33 to 2.97V?

Thank you

  • Vu Thien,

    When I open TIDM-2014, I do not see the diagram you show in your post.  So, my analysis is based on the schematic excerpt only and not the document:

    The linear operating range of an op amp is limited by its supply voltages.  This linear operating range can be limited by output-swing or common-mode specification of the amplifier.  The OPA320 common-mode is rail-to-rail ( -0.1V to 3.4V in this case).  The output swing limit depends on the load current (resistance).  In the given schematic, I assume the device is driving an ADC.  Thus, I assume the load current is fairly low.  You can look at the OPA320 output swing specification to see how close the amplifier can swing to the supply rails.  In this case, it is 10mV typical and 20mV maximum (see below for RL=10k).  However, this is the saturation limit of output swing.  As you approach this limit the signal will become distorted.  A more conservative (low-distortion) limit can be found by looking at the AOL specification test condition.  This condition says that AOL will be good (Min =114dB, Max =132dB) when Vout is within 0.1V of the supply rails (see below).  Thus, for this circuit configuration I would expect the amplifier's worst case saturation limit to be:  20mV to 3.28V (20mV limit), and the low-distortion conservative range to be  0.1V to 3.2V (0.1V limit in AOL).

    I believe the document is likely referring to factors outside of the op amp (e.g. the input from the shunt, and the ADC limits).  The op amp itself will not have the significant limits of 0.33V to 2.97V mentioned in the image.  Op Amp Input and Output Swing Limitations document explains the concepts discussed above.

    I hope this information is helpful to you.

    Best regards, Art Kay

  • Hi Art Kay,

    Thank you for your explanation, this circuit is provided in schematic design file: TIDM-02014 reference design | TI.com and for read LEM current sensor.

    Could you please guide me on how to calculate and select components (R700, R701, R702, R703, R705 and C701, C702) for the above circuit when input +/-2.75V, output 0.33 to 2.97V?

    Thank you,

    An

  • An,

    The current sense resistor is 27 ohms, and the current is 0.1018A.  27 x 0.1018 = 2.749V (rounded to 2.75V).  The circuit's response is simulate below, and the TINA simulation files are attached.

    opa320-current-shunt.TSC

    Best regards, Art