This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA186: Extended temperature part

Part Number: INA186
Other Parts Discussed in Thread: INA190-EP, TL331-EP, TLV3012-EP, TLV3603E, INA190, TL331LV, TLV1812

Tool/software:

Hello,

1. We are currently using INA186A1IDDFR in our design whose minimum operating temperature is -40degree , do we have a similar part most likely footprint compactible which is -55 degree rated without much of price difference.

2. Similar to above query , is there a part replacement for TL331LVDBVR which is -55degree rated. Need is a single channel open drain comparator with same spec.

3. Also, part similar to TLV1811DCKR which is -55degree , need is a push pull comparator.

4. Could you suggest part with below spec ,

General Purpose opamp providing rail to rail output , -55 degree operating temperature , Max supply range 5.5V or 18V. We are using this as an non inverting amplifier.