This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS4130: Difference between THS4130IDGNR and THS4130IDGN?

Part Number: THS4130
Other Parts Discussed in Thread: THS2630

Tool/software:

Hello. I am looking to replace an obsolete PN THS4130IDGN, and the THS4130IDGNR looks like the best replacement. Are there any differences between these two part numbers? From the datasheet, it looks like there is no mention of what the "R" appended to the end means, is this just an active replacement PN made to replace the THS4130IDGN?

Best,

Austen

  • Hello Austen,

    The THS4130IDGN is the tube packaging version of the THS4130 orderable.  The THS4130IDGNR is the large tape & reel packaging version of the same THS4130 orderable.  Both devices have the same temperature grade/range.

    I will also point out we have the THS2630, which is a drop-in pin-to-pin upgrade to the THS4130.  The THS2630 has the same wide industrial temperature range, a wider supply range, and improved noise & power draw specs.

    Best,

    Alec