Tool/software:
Hi team,
Do you have fully P2P device with ADA4807-2ARMZ?
I found the OPA2863A size is different with ADA4807-2ARMZ as below?


Thanks
Lillian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi team,
Do you have fully P2P device with ADA4807-2ARMZ?
I found the OPA2863A size is different with ADA4807-2ARMZ as below?


Thanks
Lillian
The 6-pin SC-70 package would be used for the single-channel device (ADA4807-1).
AD's MSOP (RM-8) package is the same as TI's VSSOP (DGK) package.
There is no exact replacement. The OPA2863A supports ±5 supplies, but has a much lower GBW. Which parameters are important?
Hi Clemens,
Thanks for your reply.
But looks as above, MSOP (RM-8) package is not the same with TI's VSSOP (DGK) package, such as length and width.
Thanks
Lillian
Hi Lillian Liu,
As Clemens mentioned, AD's MSOP (RM-8) package is the same as TI's VSSOP (DGK) package.
The above image that you have shared is of SOIC package. The below image is the DGK package which matches length and width of RM-8.

Additionally, ADA4807-2 CP-10-9 package is same as TI's DSN package.
Thanks
Vikas J